News Releases

Timken StatusCheck® Monitoring Helps to Ensure Customer’s Pumps Keep Producing Power
Self-powered paper mill runs on resource recovery with Timken reliability-assurance technology

CANTON, Ohio: May 27, 2009 — The Timken Company (NYSE: TKR) said its StatusCheck® wireless monitoring system is helping to keep critical equipment running at one of America's most environmentally progressive paper mill operators.

Located along the Pacific coast of Washington state, Grays Harbor Paper LP (GHP) produces uncoated free-sheet paper for printing and copying applications. Products include 100 percent post-consumer recycled paper made with recovered energy called “Harbor 100.”

Through Harbor 100, GHP generates much of its own electricity by burning waste-wood from its logging inventory and other sources in steam boilers that run its own turbine generators.

GHP installed the Timken’s StatusCheck® system in October 2008 to monitor three boiler feedwater pumps and associated motors that operate the turbines. The wireless system checks operating conditions of critical components such as bearings and then issues alerts via email or text messages when it detects excessive temperatures or vibration levels. 

“We decided to monitor the feedwater pumps because they are extremely expensive, given their complex, multi-stage design, high output pressure, lower tolerances and historically high maintenance costs,” said Bob Brennand, GHP mill manager. “If a pump fails and shuts down a boiler, the cost to the mill is about $6,000 an hour.” Because backup pumps are difficult to come by and complex, Brennand notes that an unplanned outage could take the unit offline for as long as four to six weeks.

It wasn’t long before Timken’s StatusCheck system proved its value at GHP. Within four months of operation, the system notified GHP’s maintenance team of an imminent failure from a motor bearing that was wearing away. “We were able to schedule pre-emptive replacement, where in the past, the bearing would likely have failed, leading to a bigger problem with a higher repair cost and more downtime,” said Brennand.

Early savings have GHP planning to install additional StatusCheck devices to monitor other critical locations in the mill, including additional pumps, fans and equipment for which a limited number of spares is available.

About Grays Harbor Paper

 

Founded in 1993 and privately owned, Grays Harbor Paper of Hoquiam, WA (www.ghplp.com) manufactures post-consumer recycled copy and printing papers which are FSC-Certified, manufactured fossil-fuel free using energy produced on-site, which is Green-e Certified. Grays Harbor has garnered the support of environmental stewards who use its paper for reports, envelopes, high-speed printing and copy applications in the public and private sector. Employing 230 team members, Grays Harbor continues to lead the way in sustainable paper production.

About The Timken Company
The Timken Company (NYSE: TKR, http://www.timken.com) keeps the world turning, with innovative friction management and power transmission products and services, enabling our customers' machinery to perform more efficiently and reliably. With sales of $5.7 billion in 2008, operations in 26 countries and approximately 25,000 employees, Timken is Where You Turn™ for better performance.

 

 

 

 

 

 

 

 

 

 

 

SOURCE: The Timken Company

 

 

Media Contact:  Lorrie Paul Crum
Manager - Global Media and Strategic Communications
Mail Code: GNW-37
1835 Dueber Avenue, S.W.
Canton, OH 44706 U.S.A.
Telephone: (330) 471-3514 
Facsimile: (330)  471-7032
lorrie.crum@timken.com

 

Investor Contact: Steve Tschiegg
Director - Capital Markets and Investor Relations
Mail Code: GNE-26
1835 Dueber Avenue, S.W.
Canton, OH 44706 U.S.A.
Telephone: (330) 471-7446
Facsimile: (330) 471-2797
steve.tschiegg@timken.com

 

For Additional Information:
www.timken.com/media

www.timken.com/investors