News Releases

New Timken® Hygienic Bearings for Food and Beverage Plants Are a Stronger Line of Defense
Meet Timken experts at IPPE 2020 and see a full line of corrosion-resistant options to improve uptime and safety

NORTH CANTON, Ohio, Jan 24, 2020 — The Timken Company (NYSE: TKR; www.timken.com), a world leader in engineered bearings and power transmission products, is helping customers engineer a stronger line of defense in food processing plants where harsh chemicals and aggressive washdowns can spell equipment troubles. Already including corrosion-resistant and greaseless bearings, the Timken portfolio of solutions for food and beverage makers now features hygienic housed units to combat common safety hazards.

Safer by Design

Hygienic bearing design considers several factors unique to food processing such as chemical contamination related to lubricant leakage, oxidation and corrosion. It also accounts for physical contamination from foreign bodies or loose or broken machine parts. Preventing microbiological contamination from bacteria that develop in dead volumes is another point of emphasis.

Timken® hygienic housed unit bearings have been designed to comply with the most stringent industry requirements. New to the company’s line of safer solutions are:

  • Timken® Hygienic Ball Bearing Housed Units that are interchangeable with standard mounted bearings from 20 to 50 mm (3/4 to 2 in.). These units feature smooth surfaces (having no reinforced bolt holes) and are available with food-grade Solid Lube that eliminates the need for re-greasing. Standard is a metal-detectable cage that significantly improves foreign particle detection probability, and customers have the option of an optically detectable blue thermoset housing that further increases the accuracy and resolution of contaminant detection.

    Ideal for: conveyors, mixers, metal detectors, check-weighers, tumblers, slicers and breaders.
     
  • Timken® Hygienic Poly-Round® Housed Units that are engineered with a special polymer insert to prevent water ingress and corrosion (the most common failure mode for bearings in food processing plants). These plain bearing units are interchangeable with industry-standard designs from 20 to 50 mm (3/4 to 2 in.) and can outperform ball bearings where a stronger solution is needed. Optically and metal-detectable inserts are available, and an optional QuiKlean® housing helps avoid dead volume between the housing base and machinery, allowing washdown from all sides (perfect for HACCP/HARPC positions and meeting FDA food contact compliance).

    Ideal for: modular belt conveyors, dumper pivots, horizontal mixers, chillers and freezers.

Notable is that Timken hygienic housed units and Poly-Round inserts are certified according to ANSI/NSF/3-A SSI 14159-1-2014 requirements. These globally recognized standards help improve food safety by mandating the use of chemically resistant materials and by requiring that bearings are easy to clean (e.g., smooth surface, laser marked, minimal crevices). The housings and inserts are further certified as Accepted Equipment by the USDA under the Meat and Poultry Equipment Review Program.

More to See

At the upcoming International Production & Processing Expo, attendees can meet Timken experts in booth B8017 or booth A2863 to discuss a smoother operation built around more reliable bearings. In addition to hygienic designs, Timken offers corrosion-resistant ball bearings, corrosion-resistant plain bearing housed units and corrosion-resistant deep groove ball bearings that provide long-lasting performance in highly wet or contaminated environments.

At Timken.com, visitors will find approved friction management solutions for every part of the plant floor, from processing to packaging, including other power transmission products that keep food and beverage producers in motion. Customers looking to manage harsh conditions, improve machine uptime and meet the highest standards for food safety can get in touch with a local Timken representative to start the conversation.

About The Timken Company

The Timken Company (NYSE: TKR; www.timken.com) designs a growing portfolio of engineered bearings and power transmission products. With more than a century of knowledge and innovation, we continuously improve the reliability and efficiency of global machinery and equipment to move the world forward. Timken posted $3.6 billion in sales in 2018 and employs more than 18,000 people globally, operating from 35 countries.

Media Relations:
234.262.3514
mediarelations@timken.com

 

(opens in a new window)